Other Parts Discussed in Thread: LF356 1. I have opened a board in which photodiode(unknown) is connected to LF356. LF356 datasheet says it require minimum +-15V, but starngely in board it is +-5V. How does it work?
2, I am planning to interface photodiode…
Other Parts Discussed in Thread: LF356 The LF356 datasheet indicates that the max input voltage is 13mv, as such, I’ll need a higher input voltage to prevent it from giving a false trigger at LF356 output pin 6 when at off state. In the circuit below,…
Part Number: OPA828 Other Parts Discussed in Thread: LF356 , Asking on behalf of customer.
According to first page of datasheet, input bias is 10x different DGN package vs. D package.
What is driving this discrepancy?
Contact me internally if further details…
I am using an LF 356 in the non inverting mode. I have connected the offset null ckt as suggested in the TI data sheet with the wiper of the null pot connected to the +12V supply. I am using -12V, Vee on pin 4. The input voltage is 0 - 5 VDC. The gain…
Other Parts Discussed in Thread: LF356 Recently, I am debugging an ultrasonic receiving circuit as shown in Figure 1.
Due to the high impedance of the ultrasonic sensor, a JFET op-amp LF356 is used to convert the high impedance to low impedance and a second…
Part Number: TLV9061 Other Parts Discussed in Thread: LF356 Hi Team ,
What characteristics are affected and what changes occur when external force is applied to the device? Part : TLV9061IDPWR Package : X2SON(DPW)
Best regards ,
Thank you Clemens for your fast response.
I dont know from which channels the LF356 were sourrced by our manufacturer.
I measured the input pins of both devices:
Our old one (with the detent) shows no clamping, the newer ones (without detent) shows 1…
Other Parts Discussed in Thread: LF356 , LM311 I am trying to build and modify the Sine Wave Generator circuit in AN263, Figure 14, albeit with what I have on my bench (TL071s in place of LF356 and LF351, and discrete transistors in place of LM394 and 2N3810…
Hey Steve,
A typical connection is shown in page 7 of the datasheet.
A similar question was asked a couple of days ago, in which Kai also explained why there is a need for balance pins/potentiometer: https://e2e.ti.com/support/amplifiers-group/amplifiers…