Part Number: LF412-N Hi,
Customer build a simple voltage follower (buffer) circuit using the LF412CN however they observe that the output hit compliance (Max Vcc Voltage) after they adjust the input voltage below 1V (all behavior is normal above 1V…
Part Number: LF412-N Hi team,
Following Tim Green's article in Operational Amplifier Stability, part 3 of 15,on the closed-loop output impendence VS frequency curve, FIG 20, we choose the G=10 curve and on its x-axis the point 0.8kHZ, at the intersection…
Part Number: LF412-N Dear Sir,
How are you doing today?
My customer would like to know the maximum input current allowed for LF412CN/NOPB (that is on the input pins 2, 3, 5 and 6).
Please let me know if you need additional information and as always…
Hiroshi-san,
Many devices were changed including LF347-N. LF412 was chosen as sample device from that group of devices changed. The LF347 (and LF412) uses a BIFET process before and after the change. The QBS device in table means a different device…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…
Hey Dan,
LM120K-5.0/883 is indeed obsolete. I've attached the PDN.
We don't have an exact P2P replacement so I'd recommend the UA79 series as the closest alternatives.
~ Aaron
PDN 200824.pdf