Part Number: LM117HVQML We’re doing a DPA on a 5962R0722962VZA (LM117HVGWRLQMLV). Per MIL-STD-883, TM 2018, SEM is not required for planar die. Is the die fully planar with no oxide steps? Are chemical mechanical polish (CMP) processes used? Or…
Part Number: LM117HVQML-SP Hi team
Is a SPICE model available for the LM117HVQML-SP.
I've checked the product folder and all of the usual places but haven't found on yet.
Thanks!
Jim B
Part Number: LM117HVQML Tool/software: Thank you for contacting us. Please let me know again.
If the frequency is 1MHz to 400MHz and the output capacitor is 6000μF, is it possible that the PSRR will fall below 10dB?
Also, if it falls below 10dB, how…
Part Number: LM117HVQML-SP Suffix A of part number 5962R9951705V9A (LM117H MDE) means it is hot solder dip lead finish. According to TI web site the component is Green (RoHS & no Sb/Br).
What is the plating of 5962R9951705V9A terminals, materials and…
Part Number: LM117HVQML Tool/software: Please advise on ① and ② below.
① Regarding the ripple rejection rate, the "Ripple Rejection" chart shows that it is 10dB at 1MHz (max), but what happens when it is between 1MHz and 400MHz?
Will it no…
Part Number: LM117HVQML Tool/software: Thank you for your help.
If the input frequency is between 1MHz and 400MHz, is it possible that the PSRR will fall below 10dB?
If it falls below 10dB, how far will it fall?
Also, the higher the frequency, the lower…
Part Number: LM117HVQML Hi,
I'm using on a space application LM117HVGW-QML chips.
I need some information about internal thermal protection circuitry that is evoked in datasheet (SNVS357D– MARCH2006– REVISED APRIL2013).
* Which type of…
Part Number: LM117HVQML-SP Other Parts Discussed in Thread: LM117QML , LM117QML-SP hello
i have a few more questions about regulator LM117H MDE.
1. what is the thermal resistance of LM117H MDE as it in DIE configuration ?
2.is the junction temperature…
Part Number: LM117HVQML-SP Hi everybody,
I'm not managing to find mass data about the LM117HVQML-SP, in particular the SKU with part number 5962R0722902VZA. In the respective webpage ( http://www.ti.com/quality/docs/materialcontentsearch.tsp?partNumber…