Part Number: LM119 Hi,
We are using this "LM119H" part in our design for this part the pin-outs marked on the LME package configuration contradicts with the pin configuration table, Kindly help on this here with I have attached a picture from from page…
Hello Christian,
Thank you for your patience. Unfortunately, we do not have a model for the LM319/LM119, but we do have a model for the similar sister-part, the LM111.
Please keep in mind that the LM119 is faster and has a wider input range – so the LM111…
Other Parts Discussed in Thread: CSD88599Q5DC , LF147 , LF156 , LM111 , LM119 , LM139 , LM2991 , LM335 , LM75B , SN74LVC1G125 , SN54AC11 , TPS54313 Dear TI Representative,
I hope you’re doing great.
I am a Components Engineer at Raytheon Technologies supporting…
Note that Paul's comment is for the ceramic packages.
The LM119QML-SP also comes in metal can. On most amplifiers and comparators, the can lid is connected to V-. That is the case for the LM119.
Part Number: LM119QML Other Parts Discussed in Thread: LM119
Hi,
I don't understand the conditions of electrical characteristics of LM119 (SNOSBJ2B) datasheet p 5.
In line 1, for Input Offset Voltage, what is the resistance Rs which is less or equal…
Part Number: LM119QML-SP Other Parts Discussed in Thread: LM119 What is the current flowing out the GND pin when the output is off (pulled high)?
I assume some current flows to bias the internal circuits of the LM119 from V+ to the GND pin?
I am using the…
Part Number: LM119QML Other Parts Discussed in Thread: LM119 I found no information on SET-shape (topic: Radiation - heavy ion test) in any document (or elsewhere in literature) answering the following question:
- We use the LM119 with UB=+/-5V. The outputs…
Other Parts Discussed in Thread: THS4631 , LM119 Hi,
I am looking for a high speed comparator with very low input offset voltage, low propagation delay and high voltage operational capability (Supply and input differential voltage capability of >12.5 V…
Other Parts Discussed in Thread: TLV3201 , TLV3502 , LMV7235 , TLV3202 , LM119 Hello all, Would you mind if we ask LM319? <Question1> In case of V+=5V, V-=0V, the data sheet shows that Input Votage Range is Min=1V, Max=3V. If input volage will be less t…
Other Parts Discussed in Thread: LM5119 , LM119 We have an application for an interleaved-output LM5119 based on the PMP7819 reference design. The output current levels and types of loads will vary greatly, including powering up into (and/or, being connected…