Part Number: LM124 I have two different Chip Layouts for the LM124 MD8 - BARE DIE.
When comparing the two chip layouts, you can see, that the two pads which stand alone on one side ( yellow marked) are very close in layout 1 and in layout 2 they are…
Part Number: LM124 Hi Team,
Can you share the information regarding the electrical characteristics of LM124AJRQMLV for V+ = 3.3V. In datasheet only 5V and 30V available.
Regards,
Mithuna
Part Number: LM124 Other Parts Discussed in Thread: LM324B Hi Team,
We would like to ask your help regarding our customer's inquiry below.
I am looking for additional data on the LM124DG4. I got the datasheet, however it doesn't have the parameters…
Part Number: LM124
Hi Experts,
We need your assistance with our customer.
Pin number 11 of LM124 is given to -15V in our design. Can the input voltage at the non-inverting terminal (pin number 3) go up to -15.3V (0.3V less than -15V)? The datasheet…
Part Number: LM124 Dear TI team
could you confirm that the following part number:
LM124AWG/883
LM136AH-2.5/883
LM117HVH/883
LM139AWG/883
are screened as per flow indicated in pag. 7 of the pdf https://www.ti.com/lit/an/sboa141a/sboa141a…
Part Number: LM124A Other Parts Discussed in Thread: LM2902 , LM124 , , LM148 1. What do the "A, J, P, B, ..." Options mean in the part number? We used part number LM124AJ 14-pin CDIP in an amplifier design that we made back in 2000. Some customers need…
Part Number: LM124 Hello,
I have question on the LM124. If the VCC 12V supply voltage is open, and the output of Op-Amp connected to a diode (cathode side). On the other side of the diode we have about 9V (through a voltage divider network) . How do…
Part Number: LM124 Hello,
I was able to check "5962-9950403VCA" at ex-datasheet before. but now, I can't find this part number on the latest datasheet.
Please, refer to ex-datasheet which is below.
I would like to know why there is not "5962…
Part Number: LM124
Possible stress to LM124 during test
<remove personal information>: Open Provide case details or comments: Dear TI, This question relates to safety of applying current to the output of any one of the four op-amp sections of unpowered…
Other Parts Discussed in Thread: LM124 Hi Team, I have designed a negative feedback open loop opamp design using LM124 to control bus voltage and I need to generate bode plot it show the stability. Kindly help me on what need to be clicked to get bode…