Part Number: LM1875 Hello Team,
We received EOL notice on part LM1875T. While looking for Alternate I could see LM1875T/LF03 and LM1875T/NOPB are Active, thinking that the basic differentiation is on Pb-free. But apart from this, what makes them different…
Part Number: LM1875 Hello Team,
The Part LM1875T/L B 02 got Obsoleted, and the recommended replacement was LM1875T/L F 02 (just Pb-free difference). When cross checking the dimensions, I could see there are two versions of NEB package (Version A &…
Part Number: LM1875 Other Parts Discussed in Thread: LM675 , LM4675 Hi,
I plan to operate the LM1875 under dual-supply condition. Do I still need C3 in datasheet figure 2 under dual-supply condition? Is there a reference design for dual-supply operation…
Part Number: LM1875LM1875 is used for middle AMP. It can't work normal, U2 and U4 bridge FFT are prone to problems. But there is no damage when the IC is removed . Attached is the design data. Is there any problem to solve the LM1875 bridging FFT problem…
Part Number: LM1875 It is found that the FFT performance is different between different IC when tested with AP, there's a 10dB difference. What is the range of this values?
The blue line is relatively flat - around 120dB.
The red line starts at 4K…
Part Number: LM1875 Hello,
Can LM1875 be used as differential input? If so, customers require typical design circuits. Could you share such circuits, or help customers design such circuits?
Best Regards,
Amy
Part Number: LM1875 Other Parts Discussed in Thread: LM384 Hi Team,
My customer's use case is input signal is 0~2.5V sine, frequency 5Khz, DC offset is 1.25V. Can LM1875 support this?
Part Number: LM1875 Hello, my supplier sold me these integrated. They do not have the letter T, and I can not find the difference in any data sheet. It seems that it does not exist without the T.
I would like to know if there are items LM1875, instead…
Part Number: LM1875 There are 2 TO-220(NEB) packages datasheet, including NEB0005B and NEB0005E, with a bit difference in the drawing. Could you please help check how to identify which option refers to in the part number? Thank you.