Part Number: LM224A Other Parts Discussed in Thread: TINA-TI , TL3474A , LM124 , LM324 , LM224 , LM2902 Hello team,
I am supporting an application where an LM224A is oscillating - typically I would do a simulation on TINA-TI but it does not seem like…
Hello Ankit,
From your description, I drew your circuit. Is this correct?
The input signal is -13.4V peak and the gain is -3.7 therefore the theoretical output peak would be +50V. The output maximum is limited by the VOH of the op amp. You already…
Dear TI
The given answers which I got do not satisfy me.
I want to use the LM224A because the offset voltages are lower than in LM2902 types. I need a quad Opamp.
Unfortunately my Ta is 100°C (15K higher than LM224A is rated).
Fortunately…
Part Number: LM324 Tool/software: Where to find open loop input impedance and open loop output impedance of LM324 datasheet LMx24-N, LM2902-N Low-Power, Quad-Operational Amplifiers datasheet (Rev. D) - lm324-n.pdf
Hi Richard,
have you read section 2.2 of this appnote?
sloa277a.pdf
By the way, which LM324 are you using? The original LM324-N from National Semiconductors or the clone from TI?
Kai
Other Parts Discussed in Thread: LM124 Hello all of you,
I have attched the LM324N datasheet with this question. I have doubt in seeting the differntial amplifier. In data sheet a circuit is given to use LM324N as differential amplifier. The amplifier…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…