Part Number: LM231 Other Parts Discussed in Thread: LM331 can the LM231 generate a symetrical triangle wave output? and yes I need to use the VCO function since the LM566 is gone.
Part Number: LM231 Other Parts Discussed in Thread: LM321 , Dear Tech Support, for LM231AN/NOPB, VOLT TO FREQ CONVERTER, in data sheet dated SEP 2015, NOTE 7, there is,
(3) If Military/Aerospace specified devices are required, please contact the TI…
Part Number: LM231 Hi TI Team,
Currently Iam working with LM231 F-V convertor.But I need one which can support frequecy atleast 100Mhz and with supply range of 3.3V.Is any F-V available with these specifications
Thanks
Sreelakshmi
Part Number: LM231 Tool/software: Hi,
the Operating junction temperature for LM231N is -20°C to 80°C. Is there a wider operating junction temperature version of LM231N? such as -40 °C to 125 °C
Part Number: LM231 Other Parts Discussed in Thread: LM358 , OPA313 Hi Sir
We need to test the frequency of the crystal oscillator , One design is count by MCU, Another design is LM231。
About LM231,Could you help to check the whole schematic? (some…
Part Number: LM231 Other Parts Discussed in Thread: LM331
Hello
We are planning to use this LM231 as V to F & F to V till 100 kHz.
While going thru' your Data Sheet. I came across this recommended Ckt.
While the rest of the Circuit is clear, what…
Part Number: LM231 Hi,
What is the storage temperature for this IC? There is no information found in the datasheet.
Thank you in advance.
Regards, Maynard
Part Number: LM231 Hi Team,
I have following request, i think answer is no but can you please confirm? Also do you think we have alternative device that can fit?
"
I will only use lm231 as IC, I have a question to ask you here. It is written on…
Part Number: LM231 Other Parts Discussed in Thread: TINA-TI , OPA340 , MAX660 , TL7660 , LM317 , OPA2340 , LM337 Hi Team,
I am a Diesel mechanic and while I have basic auto electrical and electronics understanding I don’t have the ability to design…
Part Number: LM231 I see on page 5 of the datasheet of LM231 that the definition of Non-linearity of LM231 is as below.
'Non-linearity is defined as the deviation of fOUT from VIN × (10 kHz/−10 VDC) when the circuit has been trimmed for zero error at…