Part Number: LM258A Other Parts Discussed in Thread: TS321 , , LM324A , LM258 Dear sir,
Customer wants to check whether there are ESD cell protection from Positive input (IN+) / Negative Input (IN-) to the power supply (V+/V-) inside?
AMP list:
LM258ADG…
Part Number: LM258A-EP Other Parts Discussed in Thread: LM258 Tool/software: I am using the LM258AMDREP in a scaling circuit that I am designing. The -EP datasheet for the LM258 does not list ESD ratings and I want to confirm that I can assume the same…
Part Number: OPA2188 Other Parts Discussed in Thread: LM258 Hi Support team
my customer is asking if we have OPA2188 internal circuit like following from LM258
Part Number: LM258 Hi team,
Could you share a material content report on LM258DR with PCN#20200924003.1 change ?
We need the report to get an approval from our customer so that we can deliver the product with the change.
We requested to CSC with request#CS0430676…
Part Number: LM258 Other Parts Discussed in Thread: TLV314 Hi team,
Below is LM258 SCH. We can see, if it work, LM258 U1 is output 0.5V. But actually it output 0.53V. When remove R492, it output=0.5V normally.
Keeping R392 in the board, I let U2 , U3…
Part Number: LM258 Other Parts Discussed in Thread: INA180 Hi Sir,
I am trying to make a battery current sensing circuit using LM258.
. Problem Statement- At no load condition also, the output of circuit is showing 3.8V. My requirement is for input…
Part Number: LM258 Hi Team
Customer are wondering whether the gain would be influenced when PCB has tiny distortion. The input pin 2,3 voltage keeps same as designed, while output pin1 drifts from designed. so i am trying to find any hints for such abnormal…
Part Number: LM258 hi team:
1. Please help to review the schematic
2. The power supply voltage input is 24 V, and the signal voltage input is 0-3.3 v
3. The defective products are sent to the terminal customers after the normal trial production (including…
Part Number: LM258 Other Parts Discussed in Thread: LM358B Hi team
Here customer use LM258 for two temperature sensing, but found these two temperature sensing circuit would interfere each other when using signle supply operation. However with postive…
Part Number: LM258 Hi Team:
There is a negative voltage issue on LM258 (Non-inverting amplifier) V+pin around -1V during 0.54ms_(>-0.3V) ,waveform as below
Please help below question that customer feedback , thanks. (LM258 datasheet www.ti.com/.../LM258…