Part Number: LM2901 Other Parts Discussed in Thread: LM339 , LM339LV Tool/software: In datasheet It is stated as follows. The upper end of the commonmode Voltage range is VCC+ – 1.5V; however, one input can exceed VCC, and the comparator provides a proper…
Part Number: LM2901 Hello,
Please help with the open questions on the LM2901M/NOPB NiPdAu finish.
What is the Plating Process [Electroplate, Immersion, Hot dip, Other]?
What is the Plating Heating [Fused, Annealed or None]?
Part Number: LM2901 Dear Mr. Mrs:
Besides the automorive grade, I would like to know if there are other differences between the LM2901AVQPWRQ1 and the LM2901PWR.
Thank you
Part Number: LM2901 Tool/software: Hi Team,
I found that LM2901 spec shows 1.3us response time for LM2901 and 1us response time for LM2901B.
But below curves show ~1us at the same test condition, does below curves only apply to LM2901B? Do you…
Part Number: LM2901-N Hello, can you please assist me by confirming some technical data for part number LM2901M/NOPB.
•What is the termination finish [pure Sn, matte Sn…]?
•What is the Plating Process [Electroplate, Immersion, Hot dip, Other]? …
Part Number: LM2901-Q1 Other Parts Discussed in Thread: LM2901 Tool/software: Hi,
How to perform the worst-case analysis of LM2901-Q1 considering the min to max temperatures (e.g. -10 deg C to 75 deg C)?
Part Number: LM2901 Tool/software: Dear Support Team. Page 13 of the data sheet RevX shows the supply current for LM2901's 4 channels. At Ta=25° and VCC=5V, it is Typ: 0.8mA, Max: 2.0mA. At Ta=25° and VCC=30V, it is Typ: 1.0mA, Max: 2.5mA. so it has a…