Hi Rock,
That is better. but you could also use a split resistor divider along with the diode to divide the signal further to be within the common mode range. Please see section 2.9.2.1 in Application Design Guidelines for LM339, LM393, TL331 Family Comparators…
Part Number: LM2903 Other Parts Discussed in Thread: LM393LV Hi, TI expert.
The customer applied LM2903 and configured the CT current value overcurrent detection circuit, but there are the following problems.
Problem: Even though IN- does not exceed IN…
Part Number: LM2903 Hi experts,
My customer is planning to use the LM2903PWR. They has heard that the ICs with plating of NIPDAU or SN are delivered at random, and they are worried about the visual difference between the two types of plating materials…
Part Number: LM2903
Dear expert.
My customer will face the shortage because of these Shanghai situation, but we want to use your products.
So we think to use LM2903VQPWRG4 for alternative.
The differences is only the following supply voltage as we can…
Part Number: LM2903 Other Parts Discussed in Thread: , LM393B Hi everyone, can I check about the difference in both the frame of the part between different country of origin and also the die revisions?
We first observe the difference at the lead frame…
Part Number: LM2903-Q1 Other Parts Discussed in Thread: LM2903 Team,
I'm assuming that the LM2903's output is high impedance when unpowered, but don't have one here in the lab to double check. Can you please confirm?
Thanks!
Greg
Part Number: LM2903 Hello,
What is the maximum voltage that can be input to the IN+ pin when the customer uses the LM2903 under the following conditions? Can it be used up to +30V?
- VCC = +5V
- IN- = +2.5V
Thank you.
JH
Part Number: LM2903LM2903QPWRQ1
Regarding 6.7 Switching Characteristics of spec data sheet
What is the max value of Response time 100-mV input step with 5-mV overdrive 1 . 3 ?
Part Number: LM2903 Hello team,
Can you give me the current value of test condition?
I saw jesd78 is used for Latch-up test on qualification summary, but I could not find the detailed test condition such as current value.
Best regards,
Shotaro
Part Number: LM2903 Dears,
My customer want to get the chemSHERPA version 2.5 document of LM2903DGKR, could you kindly advise where they can get such document?