Part Number: LM2903-N Other Parts Discussed in Thread: LM2903 , LM393-N , LM239 , LM393 , LM239-N Hi,
It seems that these two devices have the same parameters but LM2903(with or withoutB) is much cheaper.
The same question applies to LM239 with LM239…
Part Number: LM2903-N Dear e2e Team,
In the Figure 4 and 5 of the datasheet the logic presented is: IN+ bigger thet IN- => Output Q8 open => OUT 5V IN- bigger thet IN+ => Output Q8 close => OUT 0V
However, In the Figure 13 the logic presentesd is…
This is not the LM2903 but the LM2903-N, which was acquired from National Semiconductor. The die did not change.
As shown on ti.com/material-attributes-search/?material=LM2903MX/NOPB , there are three assembly sites.
Only the LM2903 and LM2903-N match these requirements.
As bipolar devices, the LM2903(-N) consume about 0.8 mA (total for both comparators). If you want to use a power-saving CMOS device like the TLV1822 or TLV1702, you need to use an SMD-to-DIP adapter…
Part Number: TL331 Other Parts Discussed in Thread: , LM2903-N hi teams:
1.For TI part with MPN TL331KDBVR, we encountered 100% ICT test failure, all failed material Device Marking is TIKG, after performed the material swap validation, the failure symptom…
Part Number: TPS3852-Q1 Other Parts Discussed in Thread: TPS3852 , TPS3703 , TPS3702 , LM4041-N , LM2903-N I have a question about the WDI minimum pulse duration spec.
Is it referring to 't' or 'd' in the picture below:
Hello Gabriel,
The "maximum" current would be dictated by the power dissipation and the maximum allowable VOL swing.
VOL ("saturation voltage") depends on the load current, and is shown in figure 8 (page 9) of the LM2903-N datasheet curves.
The…
Part Number: LM2903 Other Parts Discussed in Thread: LM393LV , TLV7211 , LM339 , , TLV1851 , LM4040-N , TLV6703 , TL331B Hi,
I hope you are doing well. I would like to use Texas Instruments LM2903 IC for the purpose of monitoring the voltage level of…