Part Number: LM4040-N Other Parts Discussed in Thread: LM4040 , LM2903 I think that condition of LM4040 operate(output) is reach 60μA current, but LM4040DIM3-2.5 was not operate even if current flow 174μA by external resister.
Please let me know about…
Part Number: TLV3501 Dear team,
As part of an internal review to evaluate the feasibility of extending order lead times up to 52 weeks for selected critical parts, we are gathering confirmation on supplier commercial and operational constraints.
Could…
Part Number: LM2901 Other Parts Discussed in Thread: LM339A , LM339 , LM3302 , , LM139-N , LM239-N , LM2903 , LM2903-Q1 Hello,
It seems like there is some conflicting information about the maximum temperature allowed during operation of this device…
Part Number: LM2907-N Other Parts Discussed in Thread: LM2917-N , OPT101 , LM2903 Hi Team,
my customer is looking for 50Hz/60Hz detector for Fluorescent lamp flicker detection, I make proposal below and would like to check if LM2907-N is the right solution…
Hello Eggsy,
What are the input signal voltage levels? Are any above 11V? What is the pull-up resistor value?
The LM393 and LM2903 are practically the same. Are they mixing the TI and National (-N) versions?
Hi Stanley,
Please reference pages 8 and 9 on the tech note that I have attached for more information on ESD diode clamping. Additionally, you will not need to worry about phase inversion.
Regards,
Joe
snoaa35.pdf
Part Number: LM339 Other Parts Discussed in Thread: TL074 , LM2903 , TL072 , LM311 , LM319-N Hi everybody!
I'm trying to find out how to enlarge the built-in hysteresis voltage of LM339 when comparing two different varying (AC) voltages at + and - inputs…
Other Parts Discussed in Thread: LM2903 I want datasheet for below part number.
Flex P/N
Des
Manufacturer AML
MPN Correction
TPK4H-832447-0310
IC COMPARATOR LP DUAL 8-SOIC
TEXAS INSTRUMENTS INC
SN393DR
Please help me…
Part Number: LM2903-Q1 Other Parts Discussed in Thread: LM2903 , LM393-N , LM393 , Hi Expert,
I have a question about LM2903 unused pins.
My customers are using only one of the LM2903 2in1, unused part 6PIN = open, 7, 8PIN = GND short circuited. …