Hello Eli,
The LM358 is one of a few that match the requirements you are looking for. To find possible replacements I used the TI Selection Tool under the "Compare" tab and filtered for the following:
Package Group: VSSOP
# of Channels: 2
I have…
Other Parts Discussed in Thread: TLV2760 , LM2904 Hello,
May i know the Difference between Supply Current IDD and Is that is in DataSheet. And it is belonging for single Channel or Device.
Hello,
In the Part LM2904 MWC MCD0950A, may i know what MWC MCD0950A represents to?. Shall i take the Die Size in the link http://www.ti.com/lit/ml/snao363/snao363.pdf for LM2904M part number. And in the same link i found 244µm as Mini pitch. Does it refer…
Swati,
VIO is in the range of +/-VIO[max]. It can be positive or negative with no correlation channel to channel.
IIB is always negative (conventional current flow out of the LM2904) and not zero. The minimum is -5nA. All four inputs will have a similar…
Hi Miranda,
Unfortunately, there is no model specifically for the LM321. The model used to simulate this device is the LMx58_LM2904 TINA-TI Macro model listed under the "Design and Development" section of the product page.
Regards,
Daniel
Part Number: LM2904V Hello,
C ould you help give me on LM2904V and LM2904AV spec as below ? I couldn’t find the detail spec from datasheet on ti.com, it would be good if you can share me updated datasheets.
P/N
V OS (MAXIMUM
AT 25°C)…