Part Number: LM2907-N Hello,
Could you please let me know your recommended part for following customer conditions?
Fin : 0 ~ 150Hz
Vcc = 5V (single) (If you cannot recommend 5V supply, customer can use 12V supply)
Customer want to use 8pin package device…
Part Number: LM2907-N Dear sir,
we have testes the above LM2907-M of frequency to voltage converter with a input from frequency analyzer with an input of square wave of duty cycle 50% and a VCC of 5v with is we got an output which is varing with the frequency…
Part Number: LM2907-N Hello. Simple question, I think. What is the lowest operating voltage of the LM2907? I may be incorrect, but I cannot determine this from the data sheet. Thank you.
Part Number: LM2907-N Can LM2907M-8 be replaced LM2907M-8/NOPB on same circuit?
No need to redsign circuit?
And I am planing to LM2907M-8 or LM2907-8/NOPB mount to our new design circuit.
So, I'm afraid that whether end of production is planed or not…
Part Number: LM2907-N Hello,
I am looking for datasheet of part SN29736P. The web does not recognizes that part.
Whole internet is hungry for datasheet of this part.
The problem is, that the contacts connection is uknown to me, so I do not know, if is…
Part Number: LM2907-N Other Parts Discussed in Thread: VFC32 , LM331 Hello,
Does this part work for a non-AC input signal? I am trying to convert a DC input signal that swings from 0-3V from frequencies 15-225Hz at a 50% duty cycle.
This is the datasheet…
Part Number: LM2907-N Confused on the meaning of this wording in Section 10.2.1.2.1 Choosing R1 and C1. "The output current at pin 3 is internally fixed and therefore VO/R1 must be less than or equal to this value".
I would think that if I have…
Hello Furqan,
The LM2907-N is usable with supply voltages of 6 V to 24 V so a Vcc of 12 V is good. The LM2907-N when powered by a single, positive supply must have an input that crosses below 0 V by a small negative amount to activate the input comparator…
Hi Brandon,
We haven't tried what you are thinking about doing. You will note that LM2907-N pin 8, for the 8-pin device shows an internal ground symbol. If you bias it at +2 V, then that becomes the LM2907-N's ground potential. I believe that the external…