Hi Hardy,
Unfortunately, we do not have simulation models for L M2907 and LM2917. For design procedure, please see section 10.2.1 of datasheet - see following link: https://www.ti.com/lit/ds/symlink/lm2917-n.pdf?ts=1645626893219&ref_url=https%253A%252F…
Hi Neha,
Neha Sawade said: difference between 8PIn version of LM2907 and 14 Pin Version of same LM2907 IC.Not LM2917
The differences are shown in the captured image below. If you want to read about these differences, please see AN-162 application…
Hi Robert,
Robert de Boer said: Here is something I found, must replace AFE with processsor to detect, scale and output. Robert de Boer said: Please let me know if you have a microprocessor that fits these requirements.
Please submit an inquiry to…
Part Number: LM2907-N "Two options (8-pin LM2907 and LM2917) have one input internally grounded so that an input signal must swing above and below ground and exceed the input thresholds to produce an output." is written
in the datasheet "LM2907 and…
Hello Luis,
If you are using the LM2907-N in the 8-pin package note that in datasheet Section 9.4.1 it states:
9.4.1 Grounded Input Devices (8-Pin LM2907 and LM2917)
These devices have one of the two Schmitt-Trigger comparator inputs internally…
Hi,
Regarding your LM2907N-8 questions:
1. What is the minimum supply voltage for the 2907 8-pin? I saw a post on this forum saying 6 volts, but I cannot find that in the data sheet (page 5 says -28 to 28V.
The datasheet really doesn't specify the…
For anyone else who lands up here looking for LM29x7 family spice models: there are now a family of spice models for the LM2907-8, LM2917-8, LM2907-14 and LM2917-14 devices available from EasyEDA.com/editor.
There's a demonstration of the LM2907-8…