Part Number: LM321 Other Parts Discussed in Thread: TLV9301 , LM7705 I'm using the MFX version with a 12V power supply to make a 0-10V signal. It works very well with a high-impedance load, but sometimes I need to drive a load with as little as 500 ohms…
Part Number: LM321 Hi, Team
Customer prefer to know the RθJC value for the LM321MF/NOPB.
But from the datasheet, we just have the RθJA value. Could u help to provide the RθJC to us?
Thanks.
Part Number: LM321 Other Parts Discussed in Thread: TLV07 , OPA189 , OPA991 Hi there,
In the datasheet of LM321, the input offset voltage is 2mV typically. Does it mean +IN needs to be 2mV higher than -IN? Or it is possible that -IN needs 2mV higher…
Part Number: LM321 Hi,
Please help to review customer schematic.
They connect negative input to 0V and positive input to 12V, and the V+ source is P12V_STBY, they wonder why the OUTPUT voltage is 10.6V, not 12V?
Thanks!
Part Number: LM321 Hi sir,
Can someone help to explain the circuit function of LM321 as the attachment ? What is this function for ? Many thanks indeed...
Part Number: LM321 Other Parts Discussed in Thread: LMV321-N , , LMV321 , TLV9001 , TS321 , , OPA990 , OPA170 Hi All
I have having difficulty locating a supplier for the LM321MF SOT-23
Is there a newer alternative component available with the same…