Part Number: LMV321 Other Parts Discussed in Thread: LM321LV , TLV6002 , TLV9151 , TLV9001 Hi,
Customer looks for replacement for ST LMV321. His concercern is p2p(SOT23-5) and offset.
The offset of ST/LMV321 is 0.1mV(TYP). TI LM321LV is 1mV, and…
Part Number: LMV321A Other Parts Discussed in Thread: LMV321 , LM321LV Hello,
What is the correct pin-out for the LMV321AUIDBVR SOT-23 part?
Shown below is Figure 5.1, Figure 5.2 and Table 5.1 of the datasheet - the table seems to suggest 2 pin-outs…
Part Number: DRV2700 Other Parts Discussed in Thread: LM321LV , TLV9002 Hi,
I want to design a current control circuit with MOSFET and op-amp in a feedback loop. My main goal is to be able to trigger the gate of the MOSFET with an MCU and supply 12V…
Part Number: LMV321 Other Parts Discussed in Thread: LM321LV , TLV9001 I would like to use a small single opamp as a buffer monitoring battery input for a signal, the power is supplied by uC output pin, so is 3.3V, the device will be powered off most…
Part Number: OPA2333 Other Parts Discussed in Thread: TLV9001 , LM321LV , LMV321A , TLV8801 , OPA333 , Hello,
I need a voltage to current circuit to power a tiny LED from a DAC. DAC output is 0 - 2500mV. The LED has a Vf of 2.85V. Supply voltage (V…
The parts you have listed above are the closest to MAX9914 while LM321LV and LMV321A would be the lowest cost but with higher offset (+/-3mV and +/-4mV, respectively).
Part Number: LM2904B Other Parts Discussed in Thread: LM2904 , TLV9002 , LM358LV , LM321LV , TLV9001 Hello.
I am designing a differential amplifier using LM2904.
I would like to increase the gain of my current differential amplifier, but it does not…
Other Parts Discussed in Thread: LM321 , LM321LV I bought a IC LM321LVIDCKR Qty 3000pcs from TI store on 14-Jan. finally my factory informed me that around 60% doesn't work.
sales order T01074232 Lot no. : 9001067HFT
Part Number: LMC7660 Other Parts Discussed in Thread: TL071H , TL071 , LM358B , LM321LV Originally, I wanted to amplify the voltage of about 0.1V~1.0V using TL071HIDR. So when I looked at the data sheet (6.3) of the TL071H, it said that the minimum value…
The WH2004G wants the VO control voltage to be at nominally VDD − 4.2 V. Apparently, sinking current is enough to achieve that, but only because of how the WH2004G circuit happens to be implemented.
Anyway, the LM393 is just uses as an analog buffer…