Part Number: LM324 Hello,
About the LM324 datasheet, the test conditions of input offset voltage, input offset current and input bias current are all Vo=1.4V.What does the Vo=1.4V mean?
While the Vos and Iib of LM324B and LM324BA have no this…
Part Number: LM324K Hi Support team,
My customer wants to know the internal ESD diode spec for LM324K, could you please provide the spec information?
Thank you very much.
Best Regards,
Wei-Hao
Part Number: LM324KA Other Parts Discussed in Thread: LM324K Hi,
The LM324KA datasheet shows the functional block diagram. It also shows there are 4 diodes in the component (total device) in the table.
- Where are the 4 diodes in the block diagram…
Part Number: LM2902K Other Parts Discussed in Thread: LM324K , LM2902 , LM2902B Do we have the below value or information for LM2902K? I think that the datasheet does not have LM2902K information. (Is it same as LM324K?)
1. Input offset voltage drift…
Part Number: LM2902K Other Parts Discussed in Thread: LM2902-N , LM2902 , , LM2902B , LM224K , LM324K Is ESD the only difference between "LM2902-N" (PDIP package) and "LM2902KN" (PDIP package)?
Please let me know if there are any other differences.…
Sawamoto-san,
LM324K has ESD cell on inputs. LM324DR doesn't have an ESD cell. Both have a diode behaviour for input voltage that is negative. Therefore series resistance must be used to limit current if the source driving the input is not naturally…
Part Number: LM324 HI,
Now i use amplifier is LM324PWR
6.5 Electrical Characteristics for LMx24 and LM324K,Output source current is one amplifier or four amplifiers?because a LM324PWR have four amplifiers.
thank you a lot!
Red,
The highlighted extra diodes are only present in LM324K and give the LM324K higher ESD rating. The other LM324 versions do not have these extra diodes, but they have a parasitic diodes from the input PNP transistor's base to ground junction. …
Part Number: LM324 Hi,
I see 6.5 Electrical Characteristics for LMx24 and LM324K in datasheet,i do not understand output current,As shown above
for example :1.when VCC = 15V,VO=0V,i think that if VO>0, output current is sink and is not source,why…
Curtis,
We also have a 2kV ESD version, LM324K, LM2902K and LM2902KAV device that have ESD added to the input pins. All other versions only have their natural protection meaning that there are no ESD specific cells in the design. There is also the…