Part Number: LM339 Part number: LM339MX
Question:
Old data code or new date code, if we do DIE test, if the ic chips are original, there is NS logo inside, right?
Thanks
Hao Xu
Part Number: LM339 Other Parts Discussed in Thread: TLV9022-Q1 , LM393LV , TLV7021 Hi Expert,
Sorry to bother you, I'm using LM339 to detect the voltage of the circuit as shown below,
I was found there is a voltage spike on the output pin as shown…
Part Number: LM339 We are using the LM339 as an oscillator. When a Q-tip with cold spray is touched to the top of the LM339 the oscillator frequency changes. None of the other components are being cooled. The same thing happens when the entire circuit…
Hrvoje,
Since there has not been any response to this thread in a while, I will be closing it. If you need any additional support, please open a new thread.
Thanks
Chuck
Part Number: LM339-N The LM339-N data sheet (revised December 2014) page 7 appears to have full temperature values but they are not listed as such.
Please confirm that the marked section (link below) is over full temperature.
/cfs-file/__key/communityserver…
Part Number: LM339 Hello Sir,
Can i use LM339 to design the Schmitt trigger having different threshold voltages i.e, Vth=10V and Vtl=2V ? If yes, then how could i do ? Or is there any schmitt trigger IC having these threshold voltages ?
Part Number: LM339 Other Parts Discussed in Thread: , LM393 In one of my appliction I am giving following Voltage level at input of LM339
voltage at Inverting terminal= 5Vdc
Voltage at non inverting Terminal = 14Vdc
Power supply to LM339 (Vcc…
Part Number: LM339 Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models when i am trying to import netlist it is showing as invalid entry at line#69 $CDNENCSTART