Part Number: LM339-N Dear TEXAS Team, I hope this message finds you well. I Want LM339MX/NOPB this IC IBIS Model. Could you please Share Them. Thank you for your time and support. I look forward to your response. Best regards, Argus Embedded Systems.
Part Number: LM339-N Other Parts Discussed in Thread: LM339 Tool/software: Hello,
can you please advise on a customer question, asking if parts in pics with
markings LM339N-RAYC8018 (driver) and LM339N-RAYC8024 (comparator) are the same ? If not,…
Part Number: LM339-N The LM339-N data sheet (revised December 2014) page 7 appears to have full temperature values but they are not listed as such.
Please confirm that the marked section (link below) is over full temperature.
/cfs-file/__key/communityserver…
Part Number: LM339-N Other Parts Discussed in Thread: LM339 , TLV3704 Hi,
My customer is using LM339-N. He has questions about input voltage range.
Condition is V+ = 5V and V- = GND. Q1: Can we use LM339-N with INPUT+ = +1V~+9V(swing signal) and INPUT…
Other Parts Discussed in Thread: LM339-N , LM339 , LMC7215 , TLV3691 , LPV7215 , TLV3701 , TLV3401 , LP339 , TLC339 , TLC3704 , REF1112 The Output sink current of LM339-N is specified as 6mA min.
Since this part has an open collector output, does it…
Hello Mina,
The LMX339 is from Maxim. If you need the model for that device, please contact Maxim directly.
Our LMV339 or LMV339-N would be our equivalent. You can find the SPICE model under the Design tools & simulation tab in the LM339-N product…
Thank you. There seems to be a similar error in 8.2.1.2 Application Curve for LM339-N data sheet SNOSBJ3E –NOVEMBER 1999–REVISED DECEMBER 2014
The waveforms seem inverted.
Hello Anthony,
There are two versions of the LM339 - the second source LM339 from Texas Instruments, and the original LM339 from National, which is now called the LM339-N.
See the LM339-N datasheet. The datasheet only shows the Theta JA as 95 (for…
Hello Holger,
There was a glitch during a back-end upgrade to TI.com which knocked most of the comparator datasheets off the web.
We hope to have them restored sometime today.
Attached is the LM2901-N datasheet:
/cfs-file/__key/communityserver…