Part Number: LM385-1.2 Hello All,
My customer is using LM385-1.2 in package SOT-23.
They are now looking for the same product same package with temperature range -40°C +100°C, any comments here?
Many Thanks,
Antonio
Part Number: AWRL1432BOOST Other Parts Discussed in Thread: AWRL1432 Tool/software: Hi Expert,
I am testing \ti\radar_toolbox_2_10_00_04\source\ti\examples\Kick_to_Open project with SDK 5.5.0.2 and found error happened during running as below.
INFO [gui_core…
Francis,
There isn't a lot of differences. However, these are legacy devices and we recommend to use a newer version if possible. "-N" devices were originally from National Semiconductors before TI acquired it.
Thanks,
Prakash L
LM…
Part Number: LM4041-N-Q1 HI TI team.
I know that I is -40~85 and E is -40~125 temp.
However, the table below lists both -40~125 temp.
What is the difference between LM4041QD E M3-1.2/NO and LM4041QD I M3-1.2/NO?
Please reply to my question.
Thanks.
Part Number: MCT8316ZTEVM
Tool/software:
My team is using MCT8316ZTEVM for stall torque measurements with duty cycle from 10% to 100%.
Q2 FET that got punctured is part of the Reverse Battery Protection Circuit. My understanding is that Q2 FET gets turned…
Part Number: TDA4VM Tool/software: Hello,
I need an OpenVX node that takes two inputs in and picks one to output - similar to this: https://registry.khronos.org/OpenVX/specs/1.2/html/dd/d0b/group__group__control__flow.html#gae28d45c2a30607e420e7eac1…
Hello Mohammed,
Thank you for your post!
For starters, are you able read any device registers after power up? This would at least confirm the SPI communication is set up correctly. You can also measure the following VCAPx pins with respect to AVSS:
…
Part Number: LM317L-N Hello,
according to datasheet the reference voltage is between 1.2 and 1.3 V.
Is there a selection available with more narrow tolerance around the nominal voltage 1.25 V ?
Thank you!