Use LM43600 for your application . You may design the circuit using Webench online .
Further first order Evaluation module for the desing and implement your circuit my modifying the EVM .
---Ambreesh
I do not generally support applications with output current that low. You could use a 2 or 3 A rated device but that is overkill.
For the -3.5 V output Webench suggests LM27761 or LMZ34002.
For the 1.8 V output, Webench returned a large number of possible…
Other Parts Discussed in Thread: LM43600 I'm using LM43600PWP evaluation board to step down my output voltage. The input voltage is expected to be something between 4-12 DC volts, and the output voltage should be 3.3V. The output of this buck converter…
Do you think the LM43600 would work? I've been working with the evaluation cards since I didn't really have too much input. It looks like a good regulator for my application. I am having an issue on the bench. I posted about it here:
e2e…
Diego, We are planning to update some of the models in the future to support inverting simulations. Currently we plan to add this to LM43603, LM43602, LM43601, LM43600, LM46002, LM46001, LM46000 in the near future. Some of these parts can be used as…