Other Parts Discussed in Thread: LM49450 Hi Team,
This question is in regards to the LM49450.. There is the supply voltage (Vdd, LSVdd), headphone supply voltage (CPVdd, HPVdd), digital core supply voltage (DVdd), and the digital IO supply voltage (IOVdd…
Can someone from TI please provide the leakage current for all Digital Inputs (ISS and I2C)?
Is it assumed that the "DEFAULT" register settings are the settings after every Power up (Power cycle)?
Then if the above is true, does the ISS bus…
Part Number: MSP432E401Y Other Parts Discussed in Thread: LM49450 Tool/software: Code Composer Studio Hello again,
1. The example "i2c_mastermode_simple_transfer.c" does not work.
2. I got the example working by registering the IRQ handler …
Part Number: TLV62568 Other Parts Discussed in Thread: LM49450 Hello
Do we have TLV62568DBVR and LM49450 Tc information? Customer need these data for thermal simulation. Thank you.
BR
Patrick
Shani,
This device was developed by National Semiconductor and some of the documentation is a little lacking. I am unable to locate specific data for the LM49352, but this device was developed on the same process node, and by the same team as the LM49450…
Other Parts Discussed in Thread: LM49450 , DM385 Goal : Source an external 27.576 MHz Crystal connected to AUXOSC (OSC1) to McASP2
Issues : Cannot switch McASP2 clock source.
Background :
The DM8148 board using a LM49450 Stereo DAC with Class D AMP. It is…
Hi Ravi : I tell you to take measurements i2s and capture images of the oscilloscope so that we can evaluate. I tell you that in the same lines I have connected the LM49450 i2s0 ( http://www.ti.com/lit/ds/symlink/lm49450.pdf ) working perfectly , so that…
Hi Fred: I have problems to initialize the TAS5711 device , attached for clarity initialization code in C, exported configuration file to " TAS570x GDE " which is used in tas5711_drv_init.c , circuit diagrams and circuit implemented .
Debug out…