Part Number: LM5121
Hi, to realize the customer requirements for a power cut solution of the design. To reduce the capacitor size I boost the input voltage to 45V and charge the buffer capacitor.
After the LM5121 includes an inrush limiter I want…
Part Number: LM5121 Hi,
Please tell me the current output rating (Iout_max) for the LM5121.
I couldn't read it from the datasheet.
Best Regards,Katsuyama
Part Number: LM5121 Other Parts Discussed in Thread: LM5171 , LM5170 Hi,
I want charge 100V lion battery with boost topology and CC-CV. Is LM5121 suitable for battery charging? If not, do you suggest any design?
Vin: 40V-56V
Charge current: 2A …
Part Number: LM5121 Dear Team,
We get a question from LM5121, the design circuit parameter and SCH is enclosed .Please deliver the message to your internal to see how to address oscillation issues under 52Vin~54Vin. Thanks
Specification
Vin=41V…
Part Number: LM5121-Q1 Other Parts Discussed in Thread: LM5121 Tool/software: I am not able to run noise simulation on LM5121-Q1 circuit in PSPICE for Ti. I have Ac/noise enabled set up , but in plot widow, noise icon never gets active.
Any help will…
Part Number: LM5121 Other Parts Discussed in Thread: LM5155 , LM5156 Hi,
We are designing a compact, battery-powered system that requires a regulated high-voltage DC output with the following specifications:
• Input: 5V
• Output: Adjustable 400V…
Part Number: LM5121 Tool/software: Dear team,
Customer use LM5121 for different watt application, but face to boot strop capacitor question during their design.
In LM5121 EVM, we use PSMN4R0-40YS MOSFET and the total gate charge(Qg(tot)) is up to…
Part Number: LM5121 Hi team,
My customer is considering to use this device as a charger. And the function they need is voltage regulation and current limit.
The spec is: the output is 48V and the limit current is 5A.
Support need:
1. Does this…
Part Number: LM5121 Tool/software: We designed a 24V to 48V solution with LM5121. The output current can be approx. 0 to 1A. There are a few damaged units with all N-FETs damaged. Most obvious damage is visible on high-side FET (package damaged). With…
Part Number: LM5121 Tool/software: When i run the simulation in TINA . Convergence problem tap popped up with a message of Component: .DBD. PLease find the simulation file in the attachment.
webench_design_17340686_4.tsc