Part Number: LM25149-Q1EVM-2100 Other Parts Discussed in Thread: LM25149-Q1 Hi team,
What are detail condition of "Free Convection Airflow" and "No Airflow"?
LM25149-Q1 EVM User's Guide states "Free Convection Airflow" at Thermal Performance…
Part Number: DS90UB953A-Q1EVM Other Parts Discussed in Thread: DS90UB953-Q1 If my MIPI clock is at 450 MHz am I okay to operate with the 832 Mbps per lane limit on the 953?
Does my 450 MHz clock mipi correspond to 900 Mbps of data total and thus 400 Mbps…
Hi Mohamed,
Mohamed Suhaib said: I connected the MCU's I2C directly to the MSP430's (USB2ANY) I2C pins on the EVM. I held the PDB of both the Serializer and Deserializer low. I used the "Example_USB2ANY_I2C_GUI" application from the USB2ANY SDK Sample…
Hi Ben
I am an engineer from Valeo. I am glad to see you reply. but I noticed that you did not understand what I mean to express.
Let me reiterate my situation. The signal path is PC->DS90UB949-Q1EVM->DS90UB928->TFT, but the resolution of my TFT is…
Part Number: DS90UB954-Q1EVM We are trying to configure FPD (V3Link) for a Pi HQ camera.
In the near term our setup is to operate at 720 30 fps, with raspivid.
roadmap: In the future we would like to operate at 1080 60 fps, with libcamera
Priority: I…
LM5149-LM25149 Quickstart Calculator_filled.xlsx
Hi Rahil, please find the attached for the values filled respect to our design. And Please advise if possible, we can connect a with an online meet for better understanding and for quicker result finding…
Part Number: TDA2PXEVM Other Parts Discussed in Thread: DS90UB954-Q1EVM Hello all,
I am using the TDA2PXEVM together with the DS90UB954-Q1EVM and I have problems getting the setup to run with a CSI2 data rate of 800Mbps. Everything works fine for 400…
Part Number: DS90UB960-Q1EVM Other Parts Discussed in Thread: USB2ANY Hi,
We have a few queries about the 960 EVM, which could not get resolved after reading the user manual.
Requesting inputs on the below.
1. Since the 960 is a dual hub, can we have…
Part Number: LP8860-Q1EVM Hello TI Team:
I got a problem about LED driver LP8860.
after power on, I set register table to be meet my setting. I also attached register table and schematic below.
After setting, I measure LED_Anode vs GND, it has 33V and…