Part Number: LM65645-Q1
Additional technical information
Hi Team,
We are validating this part and could not able to find some technical information like Efficiency vs load current graph, Line and load transient graph. Also simulations are not available…
Part Number: LM65645-Q1
Tool/software:
Hi,
This request is actually for another part number. I could not find the Datasheet for this part number. Can you please send me the datasheet for this part?
Thank you & Regards,
Peter
Part Number: LM65645-Q1 Other Parts Discussed in Thread: LM65625 , LM65635EVM Tool/software: Hi Sir,
I would like to find a 60V/3A DC-buck device to customer, it must be has the small package and low thermal resistance, when the operating freq at 2MHz…
Part Number: LM65645EVM Other Parts Discussed in Thread: LM65645 Tool/software: When the LM65645 will be available on the market? I can only find the evaluation board.
Part Number: LMR51635 Other Parts Discussed in Thread: AM62P , LM65645 , Tool/software: Hi Team,
We need two outputs DCDC converter below is our specs.
Input - 38-60V
Output - 3.3V@3.5A & 5V@1A.
Can we add transformer which will act inductor for…
Part Number: TPS54560B Other Parts Discussed in Thread: TPS54540B-Q1 , , LM65645 Tool/software: Hi Team,
I’m currently using the TPS54540B-Q1 in a well-established laser power management project that requires approximately 4A output current. The input…
Low temp and dual solution is counter to my experience.
An integrated dual solution will have greater power dissipation than two single solutions. the power dissipation of one channel influences the other channel, raising the fet resistance and increasing…