Part Number: LM7321 Other Parts Discussed in Thread: OPA2991 Hi,
i am using LM7321QMF in one of Sensor application for 2 Wheeler.
LM7321QMF is used as voltage follower in circuit.
Currently i am facing the issue of op-amp output voltage fluctuation during…
Part Number: LM7321 Other Parts Discussed in Thread: OPA2990 , OPA2991 Hi Sirs,
May I know there have any devices can support the Vin differential range up to +/-12V?
Part Number: LM7321 Other Parts Discussed in Thread: OPA551 , , XTR111 , XTR117 Hi,
I have to realize a robust output for current loop +/- 20mA. My old circuit uses an L272D as output, but it has high offsets that make the circuit inaccurate. Besides the L272D…
Part Number: LM7321 Hello team,
I'd like to know IC max operating current of LM7321 when it operates in 3.3V to estimate IC's possible max power consumption.
From the data sheet, I was able to find I_s (supply current) with 2.7V as below. Does…
Part Number: LM7321
Hi, Good day. I hope you are doing fine. Our customer is using the LM7321 and they have inquiry about the minimum voltage at IN+ pin. Kindly refer to the inquiry below. "I know for a power source there is a minimum 2.5+ VDC, but for the…
Part Number: LM7321 Hello,
My customer would like to use the LM7321 as a replacement for the MIC7300YM5 in the circuit below.
1. Is there any problem with using a cap of 1uF or more on the out pin?
2. Could you please provide an application example…
Part Number: LM7321 Customer is using LM7321 to bias some RF amplifiers and is observing large output oscillations. They selected the LM7321 because of its ability to handle capacitive loads without a RISO resistor. Adding a resistor is not desired in…
Part Number: LM7321 Hi Team,
The datasheet specifics -40°C for the cold end "Recommended Operating Conditions" (Section 7.3).
Will the decide operate down to -55°C? Will damage occur if tried? Is there a MIL-Grade options?
Thank You. …
Part Number: LM7321 Other Parts Discussed in Thread: BUF22821 Hi all,
My customer test LM7321 for their 12" TFT Vcom buffer application but think it's current not enough (compare with BUF22821's VCOM, cause noise on output video) for 6V Vcom…