Part Number: LM7321 Other Parts Discussed in Thread: TINA-TI , , THS4131 Tool/software: TINA-TI or Spice Models Maybe I'm missing something, but shouldn't the model file for the LM7321 have comments mapping the SPICE pins to the IC pins? Something like…
Dear Ron
Thank you for your reply.
I agree.
At the actual circuit, it should be added an isolation resistor.
I think the customer use this solution after all.
The simulation is an advance confirmation.
In the meantime, it is not mentioned OPA830.
About…
Other Parts Discussed in Thread: LM7321 Hey,
I need the LM7321 in SnPb. Since I know this part is only offered in NOPB, could someone suggest me an SnPb amp that is as similar as possible?
Thanks,
David
Part Number: LM7321-Q1 Other Parts Discussed in Thread: LM7321 Hello, the common mode voltage Vcm can reach supply voltage in customer application (or also overshot). Therefor customer need following parameter: - Vcm max rating (needed so that the IC will…
Other Parts Discussed in Thread: LM7321 Hi,
I designed the LM7321 as a unity gain amp and got a reduced output of 15mV.
After 20 cascaded amps it is summed to 300mV.
How can I reduce it to not more than 2mV?
Thanks in advance.
Other Parts Discussed in Thread: LM7321 I use lm7321 as voltage follower (gain1) and tie in+ pin to GND, the circuit Vcc is 3.3V, i found that output voltage is about 21mV!.
According to the datasheet offset voltage is +6mV max
Why the output voltage hi…
Part Number: LM7321 Hello All
I am using LM7321MFE/NOPB. Could you please tell me if i can use LM7321QMF/NOPB instead of LM7321MFE/NOPB?
Best Regards
Ayyaz
Other Parts Discussed in Thread: LM7321 I would like to confirm the data of LM7321/2 with a single supply.
The customer wants the data with about +12V supply.
Do you have the data with a single supply (except 2.7V)?
Or can we consult the data with +/5V…