Other Parts Discussed in Thread: LM7321 , LMH6629 Hi,
I use opamp LM7321 in a buffer configuration. It should drive 100pF capacitive load. Should I provide to connect also a resistive load in parallel with CL?
From simulation on TINA software I see that…
Part Number: OPA551 Other Parts Discussed in Thread: LM7321 , Hi,
I'm trying to drive primary winding of an isolation transformer (10uH inductance) with 2 high current op amps (following schematic). A zero-centered sinusoidal waveform is injected in R26…
Part Number: TIDA-00637 We are working on 240V EV for US standard. This design need to implement J1172 compliant. We have refer to TIDA-00637 design, and have some question about metering and GFCI design.
Can the GFCI section of the line detect the 4…
Other Parts Discussed in Thread: OPA2192 , THS3121 , LM7321 , OPA541 , OPA549 Hi Team
There is a linear power project, the design diagram is below , it use MCU DAC output the linear voltage, then use the amplifier as buffer and driver NMOS. Maybe it works…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM7321 , LM5176 Hi,
I'd like to ask you some questions about two parallel configuration of LM5176-Q1, The related old thread and reviewed schematic are as follows.
TI DR_0724_Reviewed.pdf
Could…
Peter,
Section 7.2 in the LM8272 goes into detail about how its design is tolerant to capacitive output loads.
Other parts that that match the "unlimited cap*" search terms are LM8262, LM7321, and LM8261.
HI Marko,
LM7321 and LM8261 are the closest parts in a single channel to LM8272. They come in SOT-23-5 package.
8 Pin VSSOP package is 3.00L x 3.00W x 0.97H mm, 0.65mm pitch and
5 Pin SOT-23-5 package is 2.90L x 1.60W x 1.20H mm, 0.95mm pitch
It will…
Part Number: LM7322 Other Parts Discussed in Thread: LM7321 Hi.
We have noticed a voltage (2.6V) on the IN+ when we apply 5V on the IN- and we got confused by this. is this expected behaviour and is it safe to run it like this?
BR // Per
Part Number: LM358 Other Parts Discussed in Thread: LM7321 , TL052 , LMV358 , THS4052 , TLV172 , MC1458 , TLC072 , LM7322 Hi,
I am using LM358 OPAMP to amplify 3.3V to 12V. This OPAMP capable of giving output current of 20mA.
New requirement has come load current…