Deepak,
I see two problems.
1) The LM339 common mode range does not include VCC+ 2) The comparators need an offset of about 15mV added. So 0mV input is off and 30mV is on.
High voltage (>6V) comparators with rail to rail (or VCC+) common mode range…
Other Parts Discussed in Thread: LMH6624 , TPS60400 , LM7705 , LM6211 , LM7321 , LF347 , OPA209 Hello,
I would like to know If I can use LMH6624 to convert a signal 0-10V to 0-5V. I would supply it with +12V-0V.
I have a sensor whose output is 0V to 10 V and…
Part Number: LDC1612
I have LDC1612- H coil
I want to repeat the process of finding L,Rs, Q, C values
And Plot the Graphs for L ,Q , Rs,C Vs Frequency
I know the formula for quality factors = Rp* square root of (C/L)
How to calculate Rp?
How the Values…