Part Number: LMC6041 Dear team,
LMC6041IMX is used for TIA circuits with a maximum gain of 500G.
The LMC6041 was packaged with plugins before, but later the plugins were discontinued and replaced with surface mount packaging, causing problems.
Operational…
Part Number: LMC6041 Hi TI team,
Customer has found several failures for MPN# LMC6041AIMX/NOPB (JPN# UTAS50-00639-000) which received under PO# 1852202785 (DC# 3422/Lot# 6323136ZFM) and required information listed below for further verification, kindly…
Part Number: LMC6041 Other Parts Discussed in Thread: TLV9101 Tool/software: Hello,
After reviewing the PCN#20250327000.1, have some questions about parameters that have changed.
After reviewing the modification summary, all the parameters seems to…
Part Number: LMC6041 Hi Team,
I have four questions.
-------
[Q1]
Is there a specification for the position of vias on Guard Ring?
And, can I use it without installing vias?
[Q2]
Is there a recommended pattern width?
For example…
Part Number: LMC6041 Dear Daneil,
Following picture is the test circuit and result of our measurement by using “Capacitor charging” method。In the measurement, we used a special switch. It is made by myself, The insulation resistance is 10e18 OHM. So…
Hi,
you are violating the common mode input voltage range of LMC6041. That's the reason why the signal is clippling at 5V supply voltage but not at 7V.
The input signal must be in a window between 0V and Vsupply - 2.4V.
Kai
Part Number: LMC6041 The LM6041 is used as input IC for very high gain (100Tohm) transimpedance amplifier. The noise characteristics vary between different ICs, some showing very low noise and others much noisier with large transient jumps. Need to know…
Other Parts Discussed in Thread: LMP7721 , LMC6041 Hi,
I am looking for replacement of LMC6041 (single micro power operational amplifier) and LMP7721 (low input bias current precision amplifier) at high temperature.
The above two can operate upto…
Hi Elisha,
Please check out OPA244 and LMC6041. Both these devices are available in single channel 8-Pin SO package. I've included few specs below, but I would highly recommend going over the datasheets.
Best Regards,
Bala Ravi
Thanks Mamadou.
Unfortunately from your list, only the LMC6041 (which is the one in my circuit) and OPA130 will operate from +/-5V. As I said in my original post, I do need a wide dynamic range as close to +/-5V as possible. OPA130 is faster than LMC6041…