Part Number: LMC662 Other Parts Discussed in Thread: OPA1652 , LMC6032 , LMV722 , TL3414A , TLV2314 , TLV2316 Dear Sir
I saw LMC662 have 600ohm drive capability
May I know 600ohm is a special feature in OP ?? or all of the latest TLV series OP have the same…
Part Number: LMC662 Other Parts Discussed in Thread: OPA2196 , LM6132 , OPA2192 Hello,
I just took over an amplifying circuit board with LMC662AIMX/NOPB which is supplied by +/-12V source, it's obvious that the op amp is over stressed according to the datasheet…
Other Parts Discussed in Thread: LMC6001 , LMC662 I am currently using LMC662/LMC6001 on a high impedance circuit and are getting changes in results once humidity is introduce to the PCB. Any suggestions on coating or set-up as to eliminate or reduce changes…
Other Parts Discussed in Thread: LMC662 , LMC6081 I'm seeking clarification on a note within the PSpice model provided for the LMC662 opamp. Specifically, there is a note within the PSpice model that "Asymmetrical gain is not modeled" and I'm not sure…
Other Parts Discussed in Thread: LMC662 the LMC662 datasheet said the operating range is from +5V to +15V, it also said that the positive power supply V+ is from +5V to +15V, and the negative power supply is from 0V to -10V. if I plan to use +5V for V…
Hi Hari,
I don't think that the output of this charge pump is higher impedant or shows less leakage current than the input of an ultra low input current OPAmp like the LMC662. Also, the MEMS will shurely draw much more current than the input current of…
Part Number: OPA454 Other Parts Discussed in Thread: LMC662 , OPA462 , OPA455
Dear Team,
We are using OPA454 for one of our Project.
Due to the wrong connection, the component got damaged.
OPA454 is not available with any vendor . Could you please suggest…
Part Number: OPA454 Other Parts Discussed in Thread: OPA462 , LMC662 , OPA455
Dear Team,
Could you please suggest an alternate P/N for OPA454 and LMC662EM ?
Its operating temperature range must be -40 ° C to 125 ° C.
My board will be working from…
Other Parts Discussed in Thread: RC4580 , OPA1678 , OPA2333-HT , LMC662 , LMP7702 Hi
Want to know if there is a chip available to filter 50 Hz line frequency noise.
Tried fliege notch filter using LMC 662 opamp but, was unable to effectively filter the noise…