Part Number: LMC7101 Other Parts Discussed in Thread: TLV9001 , OPA170 , , LMC7111 , TLV2711 , TLV2721 , TLV2731 Hi, does anybody know of an op-amp with lower input offset voltage, that is pin-to-pin compatible with the LMC7101A? This part has positive…
Other Parts Discussed in Thread: OPA735 , LMC7101 Hi,
I used LMC7101 or OPA735 on a project I started a few months ago and had to put aside. For one reason or another I'm not sure which I used.
Now I have three versions of the board, and I populated…
Dear, All
The customer is examining LMC7101-Q1. Vo value of "OUTPUT pin" becomes the point. Conditions: "V-=0V" and "V+=5.3V" Rl=10kOhm Full temperature range More than output voltage 4.975V
However, it became the following voltage when calculating…
Dear, All
The question about the output voltage of LMC7101-Q1. Please give me the graph of drops voltage to the output current for every Ta of the following. - Ta=-40℃ - Ta = 25℃ - Ta = 125℃ When there is no graph, the data based on other temperature…
Part Number: LMC8101 Other Parts Discussed in Thread: LMC7101 , OPA725 , TLV2771 , TLV2770 , OPA726 Hi,
Could you please provide the PCN for the LMC8101MM? Additionally please provide replacement part recommendation. Thank you!
Part Number: XTR111 Other Parts Discussed in Thread: LM358 , LMC7101 , LM2674 Hi experts.
This time i am using xtr111 to generate 0-20mA signal corresponding to the relative humidity in the environment (as per the datasheet of xtr111). Used SHT41 (humidity…
Other Parts Discussed in Thread: LMC7101 , LMC7211 , LMC7225 , TLV7211 , LMC7215 , LMC7221 Hi Team,
Our customer is looking for the comparator with SC-70 package and below pin-outs, can you help to check if we have such device? Thanks a lot!
Part Number: LMC7101 Good afternoon, I have a requirement to conformal coat the assembly in which we installed component LMC7101AIM5X/NOPB with Aptek 7503LM-PMF material. During the coating we are seeing a sever de-wetting condition on this component…
We had a unit where LMC7101 failed. V+ and Output pin was shorted. So we are trying to find what could cause it. I test it here in the lab. I do see about 8C to 10C temperature rise on LMC7101 when my V+ and V- is not there (0 V), but some amount of signal…
Other Parts Discussed in Thread: LMC7101 , TLV2721 , TLV2711 , TLV2731 , OPA170 Hello team,
Too have better performance in an old board, my customer would like to found an AOP p2p compatible with the LMC7101AIM with a better offset,
The main point…