Hi Rick, Welcome to the TI E2E Forums! The TIVA MCU on the ADS1261EVM enumerates as a TivaWare DFU, by default, once its flash memory has been erased. At this point you'll need to flash the MCU again to be able to use the EVM. To do this you'll need to…
Other Parts Discussed in Thread: EK-TM4C123GXL , LMFLASHPROGRAMMER , UNIFLASH So starting with the problem: After reading through the application note www.ti.com/.../spma075.pdf I am trying to program a custom board using the EK-TM4C123GXL on-board ICDI…
Hello Abhay,
Yes, it will go into hibernate mode.
You will have to erase the flash using the LMFlashProgrammer which would require the Stellaris ICDI from a a Launch Pad. There are posts where I have shown the connections to be made to get the LaunchPad…
Hello Shaswat,
When I asked for the CCS project, I do not mean just the C File. It means the entire directory in the workspace with all the files.
Anyways, I ran the code on my setup with my CCS project and the RED blinks as expected. I am able to…
Hello HY,
Yes we have multiple tools that are usable with TM4C:
https://www.ti.com/tool/UNIFLASH
https://www.ti.com/tool/LMFLASHPROGRAMMER
Best Regards,
Ralph
Hello Jaako,
Does not matter as long as the part selected has USB available. To be sure, select TM4C129XNCZAD device.
Also I checked UniFlash and it does not provide the USB option. Rather use the LMFlashProgrammer.