Hi Anthony,
It is my understanding that BT.1120 runs at 74.25MHz clock rate with 20 bits parallel interface(you can ground bits 17 through 20). In this case LMH0030 and LMH0031 basically do parallel to serial/de-seria conversion only and report CRC errors…
Other Parts Discussed in Thread: LMH0340 , LMH0030 , LMH0040 , LMH0050 , LMH0002 Hello,
My customer needs a solution of SDI Serializer which can realize 4K/30p.
[Q]
I think it may be realized in the following.
(A) Dual link 3G-SDI : LMH0340 * 2 + FPGA
(B)…
Other Parts Discussed in Thread: LMH0030 , DM385 Can any DM3xx series processor output SMPTE 274M (1080p30) suitable for standards-compliant HD-SDI coding and transmission eg with LMH0030 ? Various TI diagrams show an apparently glueless configuration to…
Other Parts Discussed in Thread: CLC021 , LMH0030 , LMH0040 I need to provide 720p 30 and 720p 60 serialized video output. Will either the CLC021 or LMH0030 do the job?
Other Parts Discussed in Thread: LMH0030 , LMH0031 I have applied all the voltages properly. The IO pin 6 is giving 3.3V as it is supposed to be, but other than that there's absolute no response. I have verified all the connections. Applied 27Mhz at the…
I apologize for the delayed response. This post would be better seen in the High Speed Interface Forum so I have moved it there.
The LMH0046 reclocker is essentially a low-pass filter system that passes jitter at frequencies below the loop bandwidth and…
Other Parts Discussed in Thread: LMH0030 I am looking for IC which will generate color video test pattern, output in HD-SDI format (device similar to LMH0030) with industrial temperature range
1). Yes i believe we should be able to use LMH0031 de-serializer to output Bt1120 to DM368. However; we don't have a reference design where this has been implemented. Please note LMH0031 has low, ~0.2UI, input jitter tolerance at high frequency. The…