Part Number: LMH2191 When VBAT is 5V and there is no input signal, both CLK1 and CLK2 oscillate.
Input signal = open or GND level.
Is there any solution?
Would the oscillation stop if I changed the power supply to 3.3V?
LMH2191.pdf
Part Number: LMH2191 Other Parts Discussed in Thread: CDC3RL02 Hi,
I have a few questions about the LMH2191.
Q1.I want to input an external reference signal to the LMH 2191 and output a square wave. Input : 10MHz,Sine wave Output: 10MHz,Square wave…
Other Parts Discussed in Thread: LMH2191 , CDC3RL02 Hi i use a TXCO 52MHz with 2 clock buffer LMH2191.
TCXO with no load is ok. If i connect LMH2191 on TXCO output, 52Mhz clock amplitude is divided by 2.
I try to insert in serie 1nF between TXCO output…
Hello TER,
Thanks so much for your reply! I have some further questions regarding on transceivers synchronization.
Is there any other way to feed clock source to CC1310 besides using quatz crystal?
Is there a way to synchronize two CC1310 chip…
Hi Gene,
A1. Output amplitude will depend on the load. I observed ~1.05V swing when loaded with 50ohms to GND.
A2. 10-pF to 50-pF load is mentioned in the datasheet because adding some small load capacitance will reduce the output slew rate which…