Part Number: LMH5401-SP Hello experts
My customer is performing DPA on part number 5962R1721401VXC.
They would like to know the lid seal material composition. I've found the table of materials here https://www.ti.com/quality-reliability-packaging-download…
Part Number: LMH5401-SP Hi Experts,
For the military qualified device, the –55°C to 125°C temperature range should refer to j unction temperature or ambient temperature? LMH5401-SP datasheet shows its operating junction temperature is –55…
Part Number: LMH5401-SP Other Parts Discussed in Thread: LMH5401 Hi Experts!
I'm looking for the S-parameter file corresponding to Figure 6 in the LMH5401-SP datasheet. Is that file available?
My customer would also like to know if this same information…
Part Number: LMH5401-SP Other Parts Discussed in Thread: TPS7H1101A-SP , CDCLVP111-SP Hi,
Pls share IBIS Model for below space parts:
LMH5401-SP
TPS7H1101A-SP
CDCLVP111-SP
Best Regards,
Umamahesh
Part Number: LMH5401-SP Hi guys, is the lid conductive? If so, is the lid is grounded internally or whether we need to provide a ground connection. And are there any restrictions on that connection.
Part Number: LMH5401-SP Other Parts Discussed in Thread: LM137JAN-SP , TIDA-01027 , ADC12DJ3200QML-SP , ADC12DJ3200 , LMH5401 , TIDA-01028 Hello,
I'm wondering what your thoughts might be for a space-grade solution for generating a -2.5V rail for the LMH5401…
Part Number: LMH5401-SP Other Parts Discussed in Thread: ADC12D1620QML-SP , LMH5401 Hi Amplifier experts!
My customer has an application requiring SE to differential conversion and amplification, and driving of the ADC12D1620QML-SP inputs. The signal is…
Part Number: LMH5401-SP Other Parts Discussed in Thread: LMH5401 , THS3491 , THS3217 , THS4561 To Whom It May Concern,
I am using the LMH5401-SP in a differential to single ended configuration. The measured noise figure was much greater than predicted from…
Part Number: LMH5401-SP Is the LMH5401-SP cold sparing? We plan to use this part as a DE-DE amplifier w/unity gain. We will have active signal transitions on this device when the power is removed from the part. Note that the input signals are also AC…