Part Number: LMH6321 Hi,
When we connect LMH6321 tab pin to negative rail supply(-15v).it was taking 140mA,and temperature was rising up to 40*C, when tab pin is left unconnected it was taking 30mA only .
Can you please clarify the above issue .
Reg…
Part Number: LMH6321 Hello guys,
One of my customers is considering using LMH6321 for their new products.
They have a few questions about the device.
Could you please give me your reply?
Q1. Is the output current shut down when the current is reached to…
Part Number: LMH6321 Other Parts Discussed in Thread: THS3491 Dear TI sirs,
I need to drive high voltage:10V and low voltage:-5V to the digital pins of deivce.Because the digital instrument of tester I am using only can support the maximum vih(driving…
Part Number: LMH6321 Dear all
I would like to ask range of VEF in LMH6321.
When I posted and exchanged about the leakage current of the EF pin of LMH6321 last time at E2E,
I heard that the leak current that flows to the EF pin is about sub-nA.
For example…
Part Number: LMH6321 Other Parts Discussed in Thread: BUF634A
Hi,
We're designing a unity gain buffer amplifier for a 38 kHz, 0 - 3V or 0 - 5V PWM signal. The specs aren't particularly fussy; the rise and fall times with a slew rate of 10 V/us would…
Part Number: LMH6321 Other Parts Discussed in Thread: OPA2210 Hello,
I am using eight LMH6321 PowerSO 8 package devices to provide higher current output capabilities for eight op-amps which are used for transducer excitation (Wheatstone bridges etc);…
Part Number: LMH6321 hi,
I am using LMH6321 as a buffer driver for video Line.Output of the DAC is converted to voltage and given to this IC.
Can PIN no 2 i.e, CL be left open?
If not what should be the VCL value? Its given in datasheet that via resistor…
Part Number: OPA593 Other Parts Discussed in Thread: LMH6321 , Hello,
I see from comments in the forum that the adjustable current limiting feature in opamps such as OPA593 and LMH6321 is not modeled in the TI-provided SPICE files.
It is possible to manually…
Part Number: LMH6321
Dear all,
In a previous post, a TI representative provided the following comment: ”It seems like the leakage current on the VEF pin is tested on the ATE with a range of +/- 23uA and has a typical value of 75pA.” I would…
Part Number: LMH6321 Team,
My customer wanted to know if we have any characterization data for the LMH6321 showing the part performance at -55C. The device is rated down to -40C but we are looking to understand its performance at -55C.
Regards,
Aaron …