Part Number: LMH6401 Hello E2E Experts,
Good day.
Could you please send me the S parameter file of the LMH6401IRMZT differential amplifier if possible?
Thank you in advance.
Regards,
CSC
Part Number: LMH6401 Hi!
Could you tell me, please, if i use LMH6401 with a low frequency differential 100 Hz signal, will there be any degradation of HD2, HD3 compared to 10 MHz signal?
There is a digital attenuator in the LMH6401. I was looking…
Part Number: LMH6401 Hello Team,
can you confirm that the voltage levels for the SPI interface always are 1.8V (high) and 0V (low) no matter if unipolar or bipolar power supply is used, please?
VS- = 0V connected to GND
VS+ = 5V
SPI-Bus voltages…
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: LMH6401
Hello E2E Experts,
I'm not sure if this is the best place to report this bug but the PSpice TI Component Library database has an issue with the LMH6401 Model Test Circuit. It refers…
Part Number: LMH6401 dear
At 1Ghz, the performance of HD3 is only -58dbc. is it due to the filter performance of the front end? Or is there something wrong with layout?
any advise ,thanks in andance
Part Number: LMH6401 Team-
Working on a DC coupled signal chain where the LMH6401 is the second stage subsequently driving a high-speed ADC.
What are the DC offset and drift numbers for this part? The data sheet doesn't seem to mention anything on…
Part Number: LMH6401 What is the state of the output of the LMH6401 when the device is disabled? Is it high-Z? Otherwise?
I don't see a description in the datasheet; might be a useful note to add to it.
thanks, -Steve
Part Number: LMH6401 Other Parts Discussed in Thread: LMH5401 VPP is 2V given when the differential resistance is 200 ohms. Now I supply power from 0-5V and single power supply. I want to know whether I can adjust the value of VPP by adjusting the differential…
Part Number: LMH6401 Hi Experts,
I have a customer who share an interesting topic about this RF amplifier.
The datasheet states the absolute maximum input voltage is VS- to VS+. This implies that the device may be damaged if any input signal is applied…