Part Number: LMH6401 To Whom it May Concern,
Would you provide an S parameter file corresponding to Figure 59 in the data sheet (the differential input impedance)? If you have a 4 port S parameter file for the entire part that would be great.
Thanks, …
Part Number: LMH6401 Hi!
Could you tell me, please, if i use LMH6401 with a low frequency differential 100 Hz signal, will there be any degradation of HD2, HD3 compared to 10 MHz signal?
There is a digital attenuator in the LMH6401. I was looking for a…
Part Number: LMH6401 Other Parts Discussed in Thread: LMH6518 , LMH6881 , THS770012 , THS7530 Hi team,
Could you give me alternative device of LMH6401 for lower cost option? Following is the customer requirement.
<Requirement>
- Flat bandwidth in…
Part Number: LMH6401 Other Parts Discussed in Thread: THS3491 , OPA695 Hi, I am using a Tektronix AWG70001B arbitrary waveform generator. The output of the generator is 500 mV signal ended or 1 Vpp differential. I need to amplify this signal and add DC…
Part Number: LMH6401 Hello. Are there any documents on the assembly process for the LMH6401? Our most recent batch of boards has a bunch of boards that fail at the THERMAL FEEDBACK GAIN CONTROL and the THERMAL FEEDBACK FREQUENCY control register settings…
Part Number: LMH6401 Hello,
TI part number LMH6401 states for the digital side SPI-1.1 compliant which means SDO should be tri-stated when Chips Select (*CS) is high. Could you please confirm this for me?
Thanks!
Regards, Ryan B.
Part Number: LMH6401 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Hi,
I'm having difficulty understanding the Macro files for TINA models.
For the LMH6401 how to I adjust the gain/attenuation by 1 dB steps in the…
Part Number: LMH6401 To whom it may concern,
I need to confirm the following problems quickly.
1) Can I use a potentiometer connected between VS+, VS- of (e.g. 10kOhm) and VOCM pin to find tune to output common-mode voltage of LMH6401.
2) Is the input…
Part Number: LMH6401 Wondering if it is possible to get the LMH6401 with a different default value configured for the gain? Have an application where we desire it to always be set to max gain, not min.