Part Number: LMH6401 Other Parts Discussed in Thread: DAC39J84 , TINA-TI To whom it may concern,
I would like to use LMH6401 to buffer the signal from a PMOS current steering DAC (TI DAC39J84).
I must use DC coupling in my application.
Now here is the…
Part Number: LMH6401 I'm trying to get a design working with an LMH6401 spi bus tied to a Altera MAX V PLD.
Will it harm the LMH6401 if the power to the PLD is applied first and the PLD forces 3.3 volts on the SPI bus pins well before the power is…
Part Number: LMH6401 Hello,
What is the high level output voltage of the SDO pin on the LMH6401? The datahsheet say "Powered from the main VS+ power supply, 1.8-V logic compliant", however no typical or maximum High-level output voltage are provided.…
Part Number: LMH6401 Hi team,
I'm an FAE supporting some industrial companies in Japan.
My customer uses LMH6401 and he asked me following questions.
Does input resistance change with secular change? e.g. If an LMH6401 has 85Ω, will it keep 85Ω over…
Part Number: LMH6401 Hello,
I am using LMH 6401 in ac coupled configuration to amplify the AC signal which is then followed by a RF power detector to convert the same signal into DC. I am a little bit confused with PD and Vocm Pins since i pulled PD pin…
Part Number: LMH6401 Hello,
I am using LMH 6401 in ac coupled configuration to amplify the AC signal which is then followed by a RF power detector to convert the same signal into DC. I am a little bit confused with PD and Vocm Pins since i pulled PD…
Hi Nobuhiko,
The same considerations for a regular FDA apply to this configuration. Proper input termination whether differential or single ended must be considered. The matching of resistors in your feedback branches of each amplifier is also key. Another…