Part Number: LMH6518 Dear
The LMH6518 outputs a differential voltage of 1.5/1.8V when powered on by default. According to the manual, its internal gain (LG, -20dB +8.86dB) is 0.877 under default configuration, which does not match the observed phenomenon…
Part Number: LMH6518 Tool/software:
Hi there,
In LMH6518: The potential root causes of the output offset drift issue in LG mode TI had to confess the LMH6518
has a huge offset problem with when using with DC Level above 400mV. They also said they…
Part Number: LMH6518 Other Parts Discussed in Thread: BUF802 The LMH6518 has a very high temperature after power-on. The input common-mode voltage is 2.5V, the single-ended signal positive minus negative is 0.245V, and the output voltage differential…
Part Number: LMH6518
The DS list the Absolute Maximum Ratings as below:
I have two questions,
For the SPI inputs, it seems they are not related to the VDD. So when VDD = 0, the SPI inputs can still withstand 3.6V?
For the various inputs, such…
Part Number: LMH6518 Hi, I see the maximum DC input is +/-400mV from an old post: LMH6518: The potential root causes of the output offset drift issue in LG mode - Amplifiers forum - Amplifiers - TI E2E support forums . But can't find that information…