Part Number: LMH6551 Tool/software: Hi team
We want to search for a device to replace EL4543, I think LMH6551 is good, but LMH6551 just have 1 channel.
Could you please recommend some 3 or 2 channel device to replace EL4543 (Renesas). Thank you!
Merry Christmas…
Part Number: LMH6551 Hello,
I am trying to design a highly sensitive transimpedance amplifier (TIA) system to amplify very low modulated current levels of a photodiode (order of ~10 nA peak-to-peak). This is my first time simulating/designing an analog…
Part Number: LMH6551 Dear sir,
Iam designing the differential amplifier using LMH6551 i need the Quiescent or ICC current which was not mentioned,
Thanks
Senthilkumaqr
Part Number: LMH6551
Hi all Would you mind if we asked LMH6551? Does this device have THD or distortion rate? We understand that audio OPAMPs have THD or distortion rate, however general OP AMPs and high speed OP AMPs aren't specified specification.…
Part Number: LMH6551 Other Parts Discussed in Thread: THS4561 , TINA-TI , THS4541 , LMH6550 , THP210 , THS4120 Hello:
There are sooo many options for selecting a suitable opamp for our application!
Pl see screenshot of the circuit using LMH6551.
Although we…
Part Number: LMH6551 Other Parts Discussed in Thread: THS4541 Hello
Could you review the circuit design with LMH6551?
LMH6551 is used to convert a singled end input to a differential output to be fed into ADC32J25IRGZT.
The signal bandwidth is < 100 MHz…
Part Number: LMH6551 Other Parts Discussed in Thread: THS4500 , THS4505 Hi,
D/S Figure 3 shows Gain = 1, could you provide similar data with Gain = 2 to 10 to our customers ?
Best regards,
Hiroshi
Part Number: LMH6551 Other Parts Discussed in Thread: ADS4225 , THS4541 Hi team,
I would like to ask about two things related to common mode voltage input VCM.
1, When using ADS4225 as post ADC and common mode output of ADC is routing to VCM pin of LMH6551…
Part Number: LMH6551 Hi,
I would like to use a fully differential amplifier because I want to interface with a sigma-delta ADC.
I need to know if there is a limit to the differential input voltage.
The voltage supply that I have is +-5V.
Can I have Vid…
Part Number: LMH6551 Hi, Our customer would like to connect a feedback resistor (RF1, RF2 of datasheet P.14,Figure23) value of 5 kΩ. Is there a limit to the resistance value? RG1 and RG2 are 500Ω. Best regards, Yuto Sakai