Part Number: LMH6552 Other Parts Discussed in Thread: ADC3649 , , TINA-TI , LM7705 We are using the LMH6552 with a differential output and an AV=2, to drive an ADC3649 analog input differentially using AC coupling. V+ is 6V and V- is 0V. Our target maximum…
Part Number: LMH6552 Hi TI's experts,
The simulated outputs of lmh6552 are somewhat unlike what I expected.
The positive output swings between Vcm and Vcm+2*Vamp.
The negtive output swings between Vcm-2*Vamp and Vcm.
Which are supposed to swing…
Part Number: LMH6552 Hi,
I am designing a prototype that works with differential signals. This signal passes through several components, and after an FDA driver implemented with the LMH6552, it needs to be fed into a band-pass filter, such as the one…
Part Number: LMH6552 Hi,
I am designing a prototype that works with differential signals. This signal passes through several components, and after an FDA driver implemented with the LMH6552, it needs to be fed into a band-pass filter, such as the one…
Part Number: LMH6552 Hi,
I am designing a prototype that works with differential signals. This signal passes through several components, and after an FDA driver implemented with the LMH6552, it needs to be fed into a band-pass filter, such as the one…
Part Number: LMH6552 Hi,
I am designing a prototype that works with differential signals. This signal passes through several components, and after an FDA driver implemented with the LMH6552, it needs to be fed into a band-pass filter, such as the one…
Part Number: LMH6552 Hi,
I am designing a prototype that works with differential signals. This signal passes through several components, and after an FDA driver implemented with the LMH6552, it needs to be fed into a band-pass filter, such as the one…
Part Number: LMH6552 Other Parts Discussed in Thread: THS4551 Hi,
I am designing a prototype that works with differential signals. This signal passes through several components, and after an FDA driver implemented with the LMH6552, it needs to be fed…
Part Number: LMH6552 Tool/software: Hello,
I am currently designing an ultra low noise current driver for a laser and would like to perform a clean characterization of the current and voltage noise density. I am using notably a LMH6552 for control purposes…
Part Number: LMH6552 Hello,
What is the minimum voltage that should be applied to the VCM - of LMH6552 -
while biasing it with +5V and Ground.
Regards,
Giora