Part Number: LMH6611 Figure 67 appears to be wrong; the parts I have are behaving as if there is only one back-to-back diode combination, and not two. In shutdown I have approximately 0.8V across the inputs, and am drawing about 10mA. Can you verify this…
Part Number: LMH6611 Hi Team,
I have a question about LMH6611 Vin+, Vin-, Vout impedance in disable.
From the datasheet, VIN+, VIN- impedance should be 6Mohms(typ) in disable.
How about Vout impedance?
if you have figure which shows frequency…
Part Number: LMH6611 Other Parts Discussed in Thread: OPA837 The datasheet SNOSB00K – provides guidance to use Rf between 500 ohms & 1kOhms on page 22/ Figure 68.
Is there a problem with using a higher resistance in the amplifier such as ~ 49.9K ot…
Part Number: LMH6611 Please provide the storage temperature rating for the LMH6611 - it is not in the datasheet.
There was also a previous e2e posting that was "Resolved" but did not provide an answer to this question.
We have a requirement for…
Part Number: LMH6611 Other Parts Discussed in Thread: LMH6609 , TINA-TI Hello,
Our customer wants to run TINA TI to see phase margin of LMH6611 application.
Where can we get Spice model of LMH6611?
Regards,
Mochizuki
Part Number: LMH6611 Other Parts Discussed in Thread: LMH6639 Hi Team,
I would like to know the Absolute Maximum Ratings "VIN Differential" specified value of LMH6611/2.
For example, I found that the LMH6639 data sheet has Absolute Maximum Ratings…
Part Number: LMH6611 Other Parts Discussed in Thread: THS4303 Hello,
one of my customer plans to configure 'voltage controlled current source' using OP-amp. Here we have two LMH6611 & THS4303 devices for his purpose. would you review if it's acceptable…