Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Other Parts Discussed in Thread: LMH6624 , LMH6629 Dear Specialists
My customer is considering LMH6624.
He wants to confirm minimum AOL at 10MHz.
His minimum requirement is 30dB@10MHz at all lots and temperatures.
Typical AOL is 40dB, so it has a possibility…
Other Parts Discussed in Thread: LMH6624 , LMH6629 , OPA847 , TINA-TI Dear Specialists
My customer is considering LMH6624.
The requirement is over 40dB@10MHz at all lots and temperatures.
Is it possible to use ?
I think it is difficult to achieve over 40dB…
Other Parts Discussed in Thread: LMH6624 Dear all,
I'm using an LMH6624 for a high speed transimpedance amplifier. The topology is pretty simple:
- input photodiode
- feedback resistor (which sets the gain) capacitor (to increase the phase margin) …
Other Parts Discussed in Thread: LMH6624 Dear Specialist
My customer is considering LMH6624.
He wants to use 5V single supply.
How is the electrical specification?
The datasheet only describes +/- rails.
Is this the same of +/- 2.5V spec. ?
Best regards…
Other Parts Discussed in Thread: LMH6624 I try to use LMH6624 to make a prea-amp for a piezoelectric sensor. I chose it for the wide band and low noise characteristics. I tried to use it in a traditional circuit where imput resistor is 1M or higher. Due…
Hey Jeremie,
In my simulation above you will see the current meter I labeled Ib in the feedback path of the LMH6624 that is in series with the resistor RF1 = 270k. Due to the large Ib or bias current on the inputs of the LMH6624, you will observe a large…
Other Parts Discussed in Thread: LMH6624 , TINA-TI , LMH6629
Dear colleagues,
I've been experimenting with a High gain Optical receiver circuit based on three of LMH6624 amplifier stages. The first LMH6624 stage is configured as a TIA. According to…
Other Parts Discussed in Thread: LMH6624 , TPS60400 , LM7705 , LM6211 , LM7321 , LF347 , OPA209 Hello,
I would like to know If I can use LMH6624 to convert a signal 0-10V to 0-5V. I would supply it with +12V-0V.
I have a sensor whose output is 0V to 10 V and…
Other Parts Discussed in Thread: LMH6624 , LMH6629 Hello,
currently, I'm working on a project with low noise preAmp (need to sense signals about 200uVpp). I've been gave from my supervisor (I'm a 2nd year student of electronics) the LMH6624. The project…
Hi Sean,
Thanks for the response, i only need an inverting gain of 5x at a bandwidth of ~20MHz. as this is the second stage op amp after a 100x gain using the LMH6624MA/NOPB.
I am using the LMH6624MA/NOPB to give me an inverting gain of x100 the input…