Part Number: LMH6703 Other Parts Discussed in Thread: OPA695 HI everyone!
I would be happy if you take a time and answer these questions :
Currently have a testing requirement for an HCSL differential CLK IC. Below are the key parameters:
Frequency…
Part Number: LMH6733 Other Parts Discussed in Thread: LMH6703 , Is LMH6703 the single version of LMH6733?
IF yes, could I supply LMH6703 also with a single 6V supply as LMH6733?
Part Number: LMH6703 Hi,
I am using LM6703MA as a unity gain amplifier and gain=0.8V but I observed a 500MHz oscillation noise with 500mV Vp-p at the output even after I got a 50ohm termination the input. I am using recommended RF = 390ohm. Is the noise…
Part Number: LMH6703 Other Parts Discussed in Thread: OPA695 , TINA-TI
Hi
I need to drive the LMH6703 in the SOT-23-6 package from a CML output.
The CML gate will operate from negative supplies, so the output is internally terminated 50 ohms to…
Part Number: LMH6703 Hi
I am using 2x LMH6703 in a cascade - inverting and then non-inverting.
-400mV input
gain 5x for stage 1
voltage divider between the two stages 66ohm and 33 ohm (2/3)
gain 4x stage 2.
3 ohm series resistor right at output…
Part Number: LMH6703 HI
It means LMH6703 can accept ±2V input signal at ±5V supply voltage but with a CMRR<40dB. And at ±6V supply voltage CMRR inproves respest to ±5V.
Is this understanding correct?
Regards,
L.
Part Number: LMH6703 Hello,
we currently use the LMH6703 in a different project.
For a small NFC-reader we want minimizde the component count and so we are interested to combine a differential to signle ended amplifier with the LMH6703 to convert…
Part Number: LMH6703 Hi, I downloaded the PSpice model for LMH6703C from the TI website "snom578" and I added the model to the Allegro CIS library. I created a simple circuit to test the model, however, I received an error. Here is a snapshot of the circuit…