Part Number: LMH6720 Other Parts Discussed in Thread: OPA691 Hello
An LMH6720 operational amplifier has taken the place of a CLC410 on an existing board. Ground planes located beneath the operational amplifier on the board are undoubtedly producing…
Part Number: LMH6720 Tool/software: Hello, We have replaced the CLC410 on a board with the LMH6720. See doc attached we have oscillations, which does not exist with the CLC410 mounted on the same card. Thank you for your help.
Remplacement CLC410…
Part Number: LMH6720 Hello Can you suggest an amp equivalent to the CLC410?
Is the LMH6720 the right amp to replace the CLC410?
CLC410 Fast Settling, Video Op Amp with Disable
Thank you
CLC410.PDF
Part Number: LMH6720 I have made a simulation using TISpice with LMH6720. I get som strange results where I do not know if it is a spice model error or this is real, and I have missed something in the datasheet?? I was expecting to be able to give an…
Other Parts Discussed in Thread: LMH6703 , LMH6720 , LMH6583 , LMH6574 , OPA4872 Are specs available on the output capacitance of LMH6703 and LMH6720 in disable mode?
I want to build 18 to 1 video multiplexers with 18 amps driving onto a microstrip…
Part Number: LMH6580 Other Parts Discussed in Thread: TCA5405 , TCA9536 , LMH6720 , TCA9537 Hello I wanted to replace the DG884 8 x 4 Wideband Video Crosspoint Array muxtiplexer with the LMH6580. I am missing a function on this product, the 4 DISABLED…
Hi Paul,
The LMH6738 shutdown circuitry is very similar to that of LMH6720. Here is what the LMH6720 datasheet shows:
So, you are correct in that there is an internal pull-up which ensure normal operation when Disable pin is left floating or open…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…