Other Parts Discussed in Thread: LMH7324 In one of my designs i use several LMH7324 comparators with the following power supplies: VCCI = +5V, VCCO=+3.3V and VEE = -5V. Due to the power sequencing the +3V3 starts some time after the +5V and -5V.
This power…
Other Parts Discussed in Thread: LMH7324 i have a pulse digitalization application
pulses are 10ns - 100ns with a repetetion rate of 20uS and current from photo diode is arround 500uA - 70mA so the drop accross 50ohm sense resistor would be 2.5mV - 3.5V…
Other Parts Discussed in Thread: LMH7324 Hello,
I want to use only one channel in a LMH7324 quad comparator. The power supplies will be VCCI = +5V, VCCO=+3V3 and VEE = -5V. Can i leave the power pins of the unused channels floating?
Regards,
Markus
Other Parts Discussed in Thread: LMH7324 dear TI,
find the attached design and please help me why LVDS output attempt is failing , i have done small modifications to the reference design only , for long term response i tried of using oscilloscope, even…
Other Parts Discussed in Thread: LMH7324 Dear precision amplifiers team,
For a project we are currntly looking into using the LMH7324 in a window comparator circuit, where the + input is connected to Ground. The - input can be negative with respect to…
Other Parts Discussed in Thread: LMH7324 Hello
My customer is testing a LMH7324 for using Single-ended to differential driver and has output wave-form as attached file.
As see the waveform, their output amplitude Q-/Q+ are not zero to High / High to zero…
Part Number: LM339 Other Parts Discussed in Thread: TINA-TI , LMV339 , LMH7324 , TLV3502 , LMV7219 , LMV7239 , TLV3202 , TLV3201 , LM2901 Hi,
We have selected LM339 for our application. The frequency of operation for the application is in MHz. (ranging from 1MHz…
Other Parts Discussed in Thread: LMH7324 i have a pulse digitalization application
pulses are 10ns - 100ns with a repetetion rate of 20uS and current from photo diode is arround 50uA - 70mA so the drop accross 50ohm sense resistor would be 2.5mV - 3.5V…
Hi Vladimir,
You are welcome!
You may be talking about a different application and not the 10MHz generator problem we've been talking about.
With a 7-10 ns pulse duration on the LMV7219 input, most likely the LMV7219 output will not register a valid…
Other Parts Discussed in Thread: LMH7322 , LMH7324 Hello:
I am trying to import the Pspice provided for the LMH7324 or LMH7322 but I am not able.
ADS shows me a message saying that the import was successful, but the only file that is created in my work…